1639581EN-06

HMI FDR settings

LTMCUF settings are not available in SoMove and have to be done with the HMI menu interface.

Confirm at start:

This setting lets the user choose the Restore behavior at startup. 2 options exist:

  • Confirm at start enabled/disabled,

  • FDR enabled/disabled.

Confirm at start enabled:

When the Restore service automatically starts, the user will have to choose between accepting to restore (OK) or cancelling (back button ).

Confirm at start disabled:

If “Confirm at start” is not selected, the restore is done automatically at startup. The user has 5 seconds to cancel the operation by pushing any of the 5 navigation buttons. Otherwise, after 5 seconds the Restore service will start.

Disable HMI FDR

“FDR disable” is an option to deactivate the HMI FDR services in case the user wants to use LTMCUF as a basic LTMCU. By default, the HMI FDR services are enabled.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.