1639581EN-06

Password Access

Overview

You can set a password for the LTMCU to limit access to configuration of LTMR controller parameters to authorized personnel. When a password has been set, other users can view the information displayed by the LTMCU, but cannot edit parameter values.

Entering a Password

The LTMCU password must be an integer from 0000 to 9999.

The process of entering a password is similar to editing a numerical setting.

Step

Description

1

Select Services - HMI setting - Password - Change passwd to navigate to the HMI Keypad Password parameter.

2

Press OK to step into the Password setting. The value 0000 appears by default, and is not necessarily the active password.

3

Press OK again to select the first (left-most) digit for editing.

4

Use or to increase or decrease the first digit value.

5

Press to move to the second digit for editing. Use or to increase or decrease the second digit value.

Note: Other digits remain hidden and are displayed as an asterisk.

6

Press to move to the third digit for editing. Use or to increase or decrease the third digit value.

7

Press to move to the fourth digit for editing. Use or to increase or decrease the fourth digit value.

8

Press OK to complete the entry of the new password. The LCD displays the screen for confirming the new password.

9

Repeat steps 3 through 8. When the new password is confirmed, the LCD returns to the previous (higher) level screen.

Authorizing Parameters Editing

When password protection is enabled, editing a parameter setting requires entering the password.

The process of entering a password is similar to editing a numerical setting.

Step

Description

1

Press contextual menu navigation keys to navigate to the parameter to edit.

2

Press . The screen to enter the password is displayed.

3

Press OK to select the first (left-most) digit for editing.

4

Use or to increase or decrease the first digit value.

5

Press to move to the second digit for editing. Use or to increase or decrease the second digit value.

Note: Other digits remain hidden and displayed as an asterisk.

6

Press to move to the third digit for editing. Use or to increase or decrease the third digit value.

7

Press to move to the fourth digit for editing. Use or to increase or decrease the fourth digit value.

8

Press OK to complete the entry of the password. When the password is confirmed, you can edit the parameter value.

Password Activation/Deactivation

Enter a password value from 0001 to 9999 to enable password protection.

Enter a password value of 0000 to disable password protection.

Password protection is disabled by default.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?