1639581EN-06

Navigating the Menu Structure

Overview

When the LTMCU is powered up:

  • The First setup menu is displayed when LTMR commissioning was not done.

  • The trip and alarm display is executed if the LTMR is in a trip or alarm condition.

  • The Quick View is displayed in other cases. Back to main menu by button.

Navigating Menus and Sub-menus

The example below shows how to navigate the menu structure to display the date and time settings:

Step

Description

Screen Display

1

If necessary, press on the right to access the main menu (shown here).

Press to scroll down to other menu choices.

2

When the Services menu is highlighted, press OK to enter the Services menu.

3

Press to select the Date-Time setting sub-menu and press OK to enter.

4

You can now access the date and time settings.

You can also press to return to the Services menu, or press on the right to return to the main menu.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.