1639581EN-06

Mounting a Portable LTMCU

Overview

You may need to move your LTMCU from one place to another. To do so, use the kit (reference LTM9KCU) equipped with magnets, which turns the LTMCU into a portable device. Then, position the kit on a metallic surface.

This section describes how to mount an LTMCU into the kit and how to remove it.

LTM9KCU Kit Characteristics

  • The kit consists of a casing, made of 2 symmetrical parts.

  • No tools are required to mount or remove the LTMCU from the casing.

  • 4 magnets, at the back of the kit, let you position the LTMCU on any metallic surface.

  • For your convenience, you can move the kit together with its connection cable using the cable housing on the rear face of the casing.

Mounting the LTMCU into the LTM9KCU Kit

To mount the LTMCU into the kit:

Step

Action

1

Position the LTMCU between the 2 parts of the casing.

2

Press the 2 parts until you hear a click.

3

On the rear face of the LTMCU, insert the mounting nut and tighten to 1 N•m (9 lb-in).

NOTE: Do not use the clamp which is part of the mounting fixation elements contained in the LTM CU box.

4

Connect the communication cable between the LTMCU and the LTMR controller on the RJ45 port.

Wind the cable into the kit winding:

  • Start winding the cable anti-clockwise, ensuring the cable goes behind the 4 legs that are on the edge of the 4 magnets.

  • On the last turn, use the slot on the lower right part of the casing to block the cable end.

NOTE: The cable housing allows for a 1 m (3.3 ft) maximum cable length.

1 RJ45 port

2 Communication cable

3 Legs (4)

4 Slot (to block the cable end)

5 Magnets

5

The magnets of the LTM9KCU kit enable the kit to be positioned on a metallic surface.

Removing the LTMCU from the LTM9KCU Kit

To remove the LTMCU from the kit:

Step

Action

1

Unwind the cable (if required), and disconnect it from the RJ45 port.

2

Unscrew the mounting nut.

3

Draw apart the two parts of the casing, and extract the LTMCU.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.