1639581EN-06

First Setup Menu

Definition

The First setup menu displays as follows:

  • On power-up, if the connected LTMR is not configured (first power-up or after executing a Clear all command in the Services menu), the parameters must be configured according to the connected LTMR and the Controller system config required to get the LTMCU operational.

  • On subsequent power-ups after selecting Config in the Services menu, see Menu - Services.

The LTMCU is in configuration mode in the First setup menu, see Sub-Menu Display.

First Setup Parameters

The following editable parameters need to be configured before the LTMR can be used. Note that some parameters in the following list may not be available depending on the configuration selections you make:

Level 1

Level 2

Level 3

Parameter name

First setup

Phases

 

Motor phases

Nominal voltage

 

Motor nominal voltage

Nominal power

 

Motor nominal power

Load CT ratio

 

Load CT ratio

Primary

Load CT primary

Secondary

Load CT secondary

CT multi passes

 

Load CT multiple passes

Operating mode

 

Motor operating mode

Two-step level(1)

 

Motor step 1 to 2 threshold

Two-step time

 

Motor step 1 to 2 timeout

Star-delta

 

Motor star-delta

Trip type

 

Thermal overload mode

Trip class

 

Motor trip class

FLC1 or OC1(2)

 

Motor full load current ratio

FLC2 or OC2(3)

 

Motor high speed full load current ratio

Definite O-Time

 

Thermal overload trip definite timeout

Local channel

 

Control local channel setting

Network protocol(4)

 

Communication protocol

Language

 

HMI language setting

End config

 

Controller system config required

(1) Depending on motor operating mode

(2) Depending on trip type

(3) Depending on trip type and motor operating mode

(4) For LTMR Ethernet TCP/IP only

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.