1639581EN-06

Menu - Metering Setting

Metering Setting Menu

The Metering setting menu contains the following sub-menus:

Level 1

Level 2

Level 3

Menu

Metering setting

Motor

Load CT

Ground CT

AC inputs

Motor

The Motor sub-menu contains the following editable parameters:

Level 3

Level 4

Parameter Name

Motor

Phases

Motor phases

Nominal voltage

Motor nominal voltage

Nominal power

Motor nominal power

Temp sensor

Motor temperature sensor type

Load CT

The Load CT sub-menu contains the following editable parameters:

Level 3

Level 4

Level 5

Parameter Name

Load CT

Load CT ratio

 

Load CT ratio

Primary

Load CT primary (external CT and specific ratio)

Secondary

Load CT secondary (external CT and specific ratio)

CT multi passes

 

Load CT multiple passes

Ground CT

The Ground CT sub-menu contains the following editable parameters:

Level 3

Level 4

Level 5

Parameter Name

Ground CT

Ground CT ratio

 

Ground current trip configuration

Primary

Ground CT primary

Secondary

Ground CT secondary

AC inputs

The AC inputs sub-menu contains the following editable parameters:

Level 3

Parameter Name

AC inputs

Controller AC logic inputs configuration

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.