1639581EN-06

Quick View Display

Overview

The Quick View display contains a scrolling list of dynamically changing values for pre-selected variables. Select the variables you want to display using the Services menu (see Menu - Services).

The Quick View is displayed:

  • manually, by selecting in the main menu,

  • automatically, after the main menu has been displayed for 10 seconds with no key pressed, or

  • by pressing to close a trip or alarm display.

There are 2 types of Quick View display modes: automatic scroll mode and manual scroll mode. You can switch from one to the other by pressing contextual navigation keys.

Automatic Scroll Mode

The following screen shows a Quick View display in automatic scroll mode. In this mode, each variable is displayed for a few seconds at a time.

1 Quick View display icon

2 Name of the variable currently displayed

3 Motor state

4 Short key to main menu

5 Access to manual scroll mode by pressing the associated contextual navigation key

6 Value of the variable currently displayed

Manual Scroll Mode

The following screen shows a Quick View display in manual scroll mode. In this mode, you can scroll through the list of variables using the contextual navigation keys.

1 Quick View display icon

2 Name of the variable currently displayed

3 Motor state

4 Short key to main menu

5 Contextual navigation keys; pressing them scroll to the next or previous variable in the Quick View

6 Access to automatic scroll mode by pressing the associated contextual navigation key

7 Value of the variable currently displayed

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.