1639581EN-06

Menu – FDR settings

Overview

The HMI FDR sub-menu gives access to FDR parameters.

Level 1 Level 2 Level 3
Menu Services Date-Time setting
    HMI setting
    Network
    History
    Config
    Settings
    Product ID
    Self-test
    Clear
    HMI FDR

FDR sub-menu

The HMI FDR sub-menu contains the following editable parameters.

Level 3 Level 4 Parameter name
HMI FDR Confirm at start Restore startup can be done automatically (the user has 5 seconds to cancel “Restore”) or manually (the user has to accept with “OK” or cancel with “”). If “Confirm at start” is selected, the Restore service is in manual mode.
  FDR disable Disable/Enable Restore service at startup.
  FDR backup now Start to back up LTMR memory to LTMCUF.
  FDR restore now Start to restore LTMR memory from LTMCUF.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.