1639581EN-06

Trips and Alarms Display

Overview

The Trips and Alarms Display contains a description of the most recent trip or alarm.

The Trips and Alarms display opens automatically upon a trip or alarm.

Trips or Alarms Display

The following diagram shows the elements in the Trips and Alarms display:

1 Text indicating whether a trip or alarm is displayed

2 Name of the trip or alarm currently displayed

Closing Trips and Alarms Display

The Trips and Alarms display is:

  • automatically closed after acknowledgement of the trip or alarm, that is:

    • for an alarm: automatic acknowledgement when the associated real-time parameter value conditions are no longer satisfied

    • for a trip: acknowledgement on your initiative by operating a reset (LTM R or communication reset)

  • temporarily closed on your initiative by pressing and navigating the menus. After a few seconds, it will appear again.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?