1639581EN-06

Using the Local Control Interface

Overview

The Local Control Interface consists of 5 control keys and 4 LEDs. The control keys, if active, enable you to control the LTMR. Pressing a control key sends a signal to the LTMR to activate the associated function.

The 4 LEDs provide information about the LTMR state. These LEDs are driven from the LTMR and are not related to the LTMCU state.

Control Key Functions

The label on each of the control keys depends on the label set you have inserted (see Inserting the Local Control Interface Label).

WARNING
UNINTENDED EQUIPMENT OPERATION
Proper labeling of the control keys must be validated.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

In order to explain the function of each control key, in the diagram below, the 5 control keys are labeled 1 to 5:

Control keys 1 to 3 are used to control LTM R outputs O.1 and O.2. The function of control keys 1 to 3 depends on the motor operating mode. The following table lists their functions for each operating mode:

Operating Mode

Assignment

Key 1

Key 2

Key 3

Overload

2-wire (maintained)

No action

No action

No action

3-wire (impulse)

Independent

2-wire (maintained)

Control motor (O.1)

Control O.2

Stop motor (open O.1) and open O.2 while pressed

3-wire (impulse)

Start motor (close O.1)

Close O.2

Stop motor (open O.1) and open O.2

Reverser

2-wire (maintained)

Forward run

Reverse run

Stop while pressed

3-wire (impulse)

Start motor forward

Start motor reverse

Stop motor

Two-step

2-wire (maintained)

Control motor

No action

Stop while pressed

3-wire (impulse)

Start motor

No action

Stop motor

Two-speed

2-wire (maintained)

Low speed control

High speed control

Stop while pressed

3-wire (impulse)

Low speed start

High speed start

Stop motor

For more information about operating mode and output assignments, see the TeSys® T LTMR Motor Management Controller User’s Manual.

The functions of control keys 4 and 5 are stable and do not depend on the operating mode. The following table describes the functions of control keys 4 and 5:

Control Key

Description

Key 4

Switch between local and remote mode.

Key 5

Reset the LTMR controller and clear all detected errors that can be reset.

Active/Inactive Control Keys

Control keys 1 to 5 are active or inactive according to the selected active control source. The following table describes the state of control keys 1 to 5 for each case:

Control Key

The LTMCU channel...

is the active control source

is not the active control source

1

Active

Inactive

2

Active

Inactive

3

Active

  • 2-wire: inactive

  • 3-wire: active if the value of the Stop HMI Disable parameter = 0 (Stop HMI key is enabled)

4

Depending on the value of the Control Remote Local Buttons Enable parameter:

  • parameter = 0 (disable): key is inactive

  • parameter = 1 (enable): key is active

5

Active

LEDs

In the diagram below, the 4 control LEDs are labeled A - D:

The following table describes each of the 4 LEDs:

LED

When active, indicates that:

Color

A

Output O.1 is active (see the functional description for control key 1 above)

Red or green

B

Output O.2 is active (see the functional description for control key 2 above)

Red or green

C

The active control source is the local source

Amber

D

The active control source is the remote source

Amber

You can choose whether the LEDs A and B are red or green when active by setting the Run LED color parameter in the Services sub-menu. See HMI Setting.

Active Control Source

The LTMCU can be configured as the local or remote active control source.

  • The LTMCU is the active local control source when the parameter Control local channel setting is set to HMI.

  • The LTMCU is the active remote control source when the parameter Control remote channel setting is set to HMI.

  • The key 4 allows to switch between local and remote control mode if the logic input I.6 is ON and the parameter HMI remote local buttons enable is set to Yes.

The parameters are available from the sub-menu Control Settings / Remote/Local. See Remote/Local in the Control Setting Menu.

The table below indicates if the keys are active or not depending on the LTMCU active source status and the color of the Local / Remote LEDs:

If LTMCU is...

and if...

Then the keys are...

the local active source

LED C is ON (amber)

active

LED D is ON (amber)

inactive

the remote active source

LED C is ON (amber)

inactive

LED D is ON (amber)

active

Example

The following example explains the meaning of LED C and D state to know whether keys 1 and 2 are active or not.

If the 2 following conditions are satisfied:

  • Control local channel setting parameter is set to HMI (in this example: HMI = LTMCU)

  • I.6 input is active (for example in case of a strap between C and I.6 inputs on the LTMR plug-in terminal)

Then the HMI is the local control channel and keys 1 and 2 are active / inactive according to LED C and D state:

  • LED C ON and LED D OFF means that the LTMCU is the active control source: keys 1 and 2 are active

  • LED C OFF and LED D ON means that the LTMCU is not the active control source: keys 1 and 2 are inactive.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.