About the Book
At a Glance - Document Scope
This manual describes how to install, configure and use the TeSys® T LTMCU Control Operator Unit.
The firmware version of the LTMR connected to the LTMCU must be LTMCU compliant: the LTMR firmware version must be 2.1 and above.
Validity Note
This manual is valid for all LTMCU Control Operator Units. The availability of some functions depends on the software version of the Control Operator Unit.
|
Title of Documentation |
Reference Number |
|---|---|
|
TeSys® T LTMR Modbus Motor Management Controller User Manual |
1639501 |
|
TeSys® T LTMR Profibus Motor Management Controller User Manual |
1639502 |
|
TeSys® T LTMR CANopen Motor Management Controller User Manual |
1639503 |
|
TeSys® T LTMR DeviceNet Motor Management Controller User Manual |
1639504 |
|
TeSys® T LTMR Ethernet TCP/IP Motor Management Controller User Manual |
1639505 |
|
TeSys® T LTMCU•• Instruction Sheet |
1639582 |
You can download these technical publications and other technical information from our website at www.se.com .
Proposition 65 Notice
|
WARNING: This product can expose you to chemicals including lead and lead compounds, which are known to the State of California to cause cancer and birth defects or other reproductive harm. For more information go to www.P65Warnings.ca.gov. |