1639581EN-06

Main Menu

Overview

The LTMCU’s main menu gives access to sub-menus which enable access to the parameters required to configure the LTMR. The settings sub-menus are described below:

Sub-menu

Contains

See...

Metering setting

Configurable settings for Motor, Load CT, and Ground CT parameters.

Menu - Metering Setting

Protection setting

Configurable settings for Thermal, Voltage, Current, Power and Voltage Dip Management parameters.

Menu - Protection Setting

Control setting

Configurable settings for fallback, remote/local mode, transfer mode, detected trip reset, diagnostics, motor and contactor parameters.

Menu - Control Setting

Services

Configurable settings for HMI, network, maintenance and detected trip history as well as read-only parameters for product ID. This menu also enables you to set parameters for Quick View.

Menu - Services

Language

Available languages for the LTMCU display. The default language is English.

Language Management

NOTE: Not all the parameters listed in the following pages will appear in the LTMCU sub-menus. The parameters available depend on the type and configuration of the system.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.