1639581EN-06

Selecting the Language Displayed by the LTMCU

Procedure

The procedure below enables you to select one language stored in the LTMCU memory:

Step

Action

1

Press to return to the LTMCU main menu.

2

Display the Language sub-menu by:

  • either navigating the menu structure: Menu/Services/HMI setting/Language,

  • or select the Language sub-menu from the main menu.

3

Select a language among the list of stored languages.

Up to 3 stored languages are available.

4

Use the and keys to select a language among the list of stored languages.

Press OK.

The LTMCU will now display the language you have selected.

NOTE: If you want to display another language, you can download other languages by using a PC running the LTMCU Langtool language management software: see Language Management.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.