1639581EN-06

Inserting the Local Control Interface Label

Overview

The local control interface is the part of the LTMCU that contains the 5 control keys and 4 LEDs. To identify these different elements, you can choose:

  • one of the pre-defined labels,

  • the blank label that you can customize with a pen.

The diagram below shows an example of a pre-defined label:

NOTE: The label must be chosen according to the LTMR controller's operating mode. The keys’ label on the local control interface must be appropriate to the functions of the LTMR operating mode.

Inserting Labels

To insert a local control interface label:

Step

Action

1

Slide the tip of the label into the slit on the side of the LTMCU as shown below.

Be careful to use the right slit as shown in the zoom below.

2

Slide the rest of the label into position in the LTMCU, correctly align the identifiers on the label with the interface elements.

3

Tuck the label tab into the tab loop, as shown in the diagram below:

4

Push the tab into place so it lies flat against the loop:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.