1639581EN-06

Menu - Control Setting

Control Setting Menu

The Control setting menu contains the following sub-menus:

Level 1

Level 2

Level 3

Menu

Control setting

Fallback

Remote / Local

Stop enable

LI3 assignment

Diagnostics

Trips reset

Motor

Contactor

Fallback

The Fallback sub-menu contains the following editable parameters:

Level 3

Level 4

Parameter Name

Fallback

HMI fallback

HMI port fallback setting

Network fallback

Network port fallback setting

Remote/Local

The Remote / Local sub-menu contains the following editable parameters:

Level 3

Level 4

Parameter Name

Remote/Local

Remote channel

Control remote channel setting

Local channel

Control local channel setting

HMI R/L enable

HMI remote local buttons enable

Power-up mode

HMI remote local default mode

Transfer mode

Control transfer mode

Stop enable

The Stop enable sub-menu contains the following editable parameters:

Level 3

Level 4

Parameter Name

Stop enable

Terminals

Stop terminal strip disable

HMI

Stop HMI disable

LI3 assignment

The LI3 assignment sub-menu contains the following editable parameter:

Level 3

Parameter Name

LI3 assignment

Logic input 3 external ready enable

Diagnostics

The Diagnostics sub-menu contains the following editable parameters:

Level 3

Level 4

Level 5

Parameter Name

Diagnostics

Wiring trip

Trip enable

Wiring trip enable

On-Off diagnostic

Trip enable

Diagnostic trip enable

Alarm enable

Diagnostic alarm enable

Trip Reset

The Trip reset sub-menu contains the following editable parameters:

Level 3

Level 4

Level 5

Parameter Name

Trip reset

Reset mode

-

Trip reset mode

Autoreset group 1

Reset number

Auto-reset attempts group 1 setting

Reset time

Auto-reset group 1 timeout

Autoreset group 2

Reset number

Auto-reset attempts group 2 setting

Reset time

Auto-reset group 2 timeout

Autoreset group 3

Reset number

Auto-reset attempts group 3 setting

Reset time

Auto reset group 3 timeout

Motor

The Motor sub-menu contains the following editable parameters:

Level 3

Level 4

Parameter Name

Motor

Operating Mode

Motor operating mode

Rapid cycle time

Rapid cycle lockout timeout

Direct transition

Control direct transition

Transition time

Motor transition timeout

Two-step level

Motor step 1 to 2 threshold

Two-step time

Motor step 1 to 2 timeout

Star-delta

Motor star-delta

Contactor

The Contactor sub-menu contains the following editable parameters:

Level 3

Level 4

Parameter Name

Contactor

Contactor rating

Contactor rating

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.