1639581EN-06

Parameter Display

Overview

The LTMR parameters are contained in 2 different menu structures:

  • the main menu and sub-menus

  • the First setup menu

The navigation and sub-menu presentation are identical in the 2 menu structures. Each sub-menu consists of one or several levels of nested parameters.

The main menu appears

  • on power-up of the LTMCU after the First setup menu settings have been saved, if no trips or alarms are detected, or

  • by pressing the button.

The main menu consists of 5 sub-menus: Metering setting, Protection setting, Control setting, Services, and Language. You can access each of these sub-menus from the main menu.

The First setup menu enables to set a limited number of configuration parameters of the LTMR, see First Setup Menu.

Main Menu Display

The following diagram shows the elements in the main menu display:

1 Main menu icon and title

2 Scroll bar, indicating level in the main menu

3 Short key to Quick View display (from main menu only)

4 Contextual menu navigation keys

5 Display area, with list of sub-menus identified by icon and title

Sub-Menu Display

The following diagram shows an example of a sub-menu display:

1 Menu icon and title

2 Scroll bar, indicating level in sub-menu

3 Short key to main menu

4 Contextual menu navigation keys

5 Return to higher-level menu key

6 Display area, with list of sub-menus

First Setup Display

The following diagram shows the First setup menu display:

1 First setup menu icon and title

2 Configuration mode icon

3 Scroll bar, indicating level in the First setup menu

4 Contextual menu navigation keys

5 Display area with list of accessible parameters

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.