1639581EN-06

LTMCU Physical Description

Front Face

The front face of the LTMCU is shown below:

1 LCD display

2 Contextual navigation keys

3 Front face RJ45 port for PC connection (covered)

4 Local control interface, including 5 control keys and 4 LEDs

For a detailed description of:

Navigation Keys

The LTMCU navigation keys are contextual, that is, their function depends on the associated icons shown on the LCD display. These icons change for different displays, so the navigation key functions also change.

The navigation keys can be used to:

  • navigate menus and sub-menus,

  • scroll within a value list,

  • select a setting in a value list,

  • exit a value list without making a selection,

  • return to the main (first-level) menu,

  • switch between manual and automatic presentation mode in Quick View display.

The diagram below shows an example of the different functions of each of the navigation keys associated with an icon on the LCD display:

1 Information area of the LCD display

2 Contextual navigation icons area of the LCD display

3 Move up to the next higher-level menu

4 Move down to the next item in the menu

5 Select an item

6 Move up to the previous item in the menu

7 Return to the main menu

Contextual Navigation Icons

The following table describes the icons used with the contextual navigation buttons on the LTMCU:

Icon

Description

Icon

Description

Enables access to the main menu from a sub-menu or from Quick View

Enables access to Quick View from the main menu or a sub-menu

Scroll down

Enables access to manual scroll mode (when Quick View is in automatic scroll mode)

Scroll up

Enables access to automatic scroll mode (when Quick View is in manual scroll mode)

Validates a setting or value and enables access to a sub-menu when a menu is selected

Used to increment a setting in menu mode

Move up to the next higher-level menu

Used to decrement a setting in menu mode

When a menu item is password-protected, this icon enables access to the Enter Password screen

   

Information Icons

The following table describes the icons provided as information in the information area of the LCD display. They indicate, among others, the selected menu or parameter.

Icon

Description

Icon

Description

Main menu

Indicates that the present display is Quick View

Metering setting menu

Indicates that an alarm has occurred

Protection setting menu

Indicates that an error has been detected

Control setting menu

Information

Services menu

Check box selected

Language selection menu

Check box unselected

Radio button selected

Item has been selected (for inclusion in Quick View display)

Radio button unselected

LTMR in Configuration mode

LCD Displays

The LTM CU presents 3 different LCD displays:

LCD display

Functions

Menu

  • Displaying and editing the configuration settings required for configuring the LTM R (metering, protection, control and services settings)

  • Displaying diagnostic and history data

Quick View

  • Displaying real-time metering of pre-selected parameters by automatic or manual scrolling

Trips and Alarms

  • Displaying the most recent trip or alarm

Each of these 3 displays is described in detail below.

LCD Display Settings

  • The LCD display is continuously backlit.

  • Contrast and Brightness are adjustable by using the Services menu.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.