DOCA0160EN-00

Parameter Modification

To modify the value of a parameter, follow either of the methods described below:

  • Select a value in the list.

  • Modify the numerical value, digit by digit.

Selecting a Value in a List

To select a value from the list of settings, use the menu buttons as described below:

  1. Press the and buttons to select the desired value.

  2. Press the OK button to save the selected setting value.

Modifying a Numerical Value

The numerical value of a parameter is made up of digits from 0 to 9.

To modify the numerical value, use the menu buttons as described below:

  1. Press the and buttons to modify the numerical value of the selected digit.

  2. Press the OK button to save the value of the selected digit.

    Result: The following digit is selected and can be modified as the first digit. If there is no other digit to set, the setting value is saved.

NOTE:
  • After modifying the numerical value, press the OK button to save the value.

  • To increase or decrease the numerical value at a higher speed, press the or button for a longer duration of time.

Pressing Multiple Buttons

If multiple buttons are pressed simultaneously, no action is performed and the pressed buttons are ignored except for the password reset function. Release the pressed buttons in order to press another button.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?