Hardware Description
VigiPacT RHB Relay
|
A |
Status LEDs: ON, PRE-AL, ALARM |
|
B |
Multi-functional LCD display |
|
C |
Test/UP button |
|
D |
Reset/DOWN button |
|
E |
Home or OK button |
|
F |
QR code to access device information |
|
G |
Lead-seal cover |
|
H |
Socket for toroid connection with the wiring kit |
VigiPacT RHB Toroids
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
The table below shows the list of supported toroids:
|
Toroid |
Diameter |
|
|---|---|---|
|
TB35 (LV481011) |
35 mm |
|
|
TB35P (LV481015) |
||
|
TB60 (LV481012) |
60 mm |
|
|
TB60P (LV481016) |
||
|
TB120 (LV481013) |
120 mm |
|
|
TB210 (LV481014) |
210 mm |
|
|
A |
Toroid |
|
B |
Socket for relay connection with the wiring kit |
|
C |
Test button |
|
D |
Status LED: ON/ALARM |
|
E |
Measuring range setting dial |
DANGER