DOCA0160EN-00

Setting the >I2 Alarm Threshold

Step

Action

Screen

1

Press the OK button for more than 2 s.

Result: Idn flashes on the screen.

2

Press the OK button.

Result: >I2 flashes and the value of alarm threshold is displayed on the screen.

3

Press the OK button to change the value of alarm threshold.

NOTE: If the password protection is set to on, then it is required to enter the password to change the value. Enter the password by using or button and press OK button.

4

Use the and buttons to set the appropriate value of alarm threshold.


5

Press the OK button to save the value of alarm threshold.

Result: >l2 flashes and the new value of alarm threshold is displayed on the screen.

6

To exit the current submenu, select the ESC submenu by using or button and press OK button.

Result: Idn flashes on the screen.

7

To exit the menu and display the Home screen, select the ESC submenu by using or button and press OK button.

Result: Home screen is displayed.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?