DOCA0160EN-00

Device Information

The device information (InF) menu allows you to get the information about the hardware and firmware versions. After activating this menu, the data will be displayed as a scrolling text. You can select the individual data sections by using the or button.

Step

Action

Screen

1

Press the OK button for more than 2 s.

Result: Idn flashes on the screen.

2

Press the button three times to select InF menu.

3

Press the OK button.

Result: The relay hardware and firmware versions scroll on the screen.

NOTE: Press the or button to manually scroll through the hardware and firmware versions.

4

To exit the current submenu, select the ESC submenu by using or button and press OK button.

Result: InF flashes on the screen.

5

To exit the menu and display the Home screen, select the ESC submenu by using or button and press OK button.

Result: Home screen is displayed.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?