DOCA0160EN-00

Automatic Self Test

The VigiPacT RHB relay monitors continuously:

  • the toroid connection

  • the toroid settings

  • the relay internal functions

When a malfunction is detected:

  • K1 and K2 relays are activated

  • the 3 LEDs are blinking

  • an error code is displayed on the screen. For more information, refer section Troubleshooting

    .

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?