DOCA0160EN-00

Earth-Fault Protection Function

The main functions of VigiPacT RHB relay are:

  • Measures the earth-leakage current detected by the toroid.

  • Displays the earth-leakage current.

  • Trips the installation protection circuit breaker through an MN or MX voltage release if the earth-leakage current exceeds the alarm threshold >I2 for a time greater than the time delay ton2.

  • Implements two earth-leakage current thresholds, one corresponding to a pre-alarm and another to an alarm.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.