Procedure
- Turn off the main circuit breaker in the open (O-Off) position.
- Turn off the circuit breaker of the relay in the open (O-Off)
position.Result: The toroid status LED switches off.
- Press the Test button on the toroid and maintain it pushed.
- Turn on the circuit breaker of the relay in the closed
(I-On) position.Result: The toroid is ready for calibration when the status LED of toroid blinks red slowly.
- Release the Test button on the toroid
to start the calibration.Result:
-
the status LED of toroid blinks red quickly during the calibration.
-
the status LED of toroid turns steady green when the calibration is finished.
-
The message E.01 is displayed on the relay. The 3 LEDs on the relay blink and the pre-alarm relay K1 and alarm relay K2 change state.
-
- Press the Reset button on the relay.Result:
-
The Home screen is displayed on the relay. The 3 LEDs on the relay stop blinking and the pre-alarm relay K1 and alarm relay K2 change state.
-
The relay is ready for operation.
-
- Close the main circuit breaker.