DOCA0160EN-00

Activating the Password Protection

Step

Action

Screen

1

Press the OK button for more than 2 s.

Result: Idn flashes on the screen.

2

Press the button two times to select SEt menu.

3

Press the OK button.

Result: The lock icon flashes and the password setting OFF is displayed on the screen.

4

Press the OK button to change the password setting to on.

5

Use the and buttons to change the password setting to on.

6

Press the OK button.

Result: The existing password flashes on the screen.

7

Use the and buttons to enter the new password.

8

Press the OK button to save the new password.

Result: Lock icon flashes and the password setting on is displayed on the screen.

9

To exit the current submenu, select the ESC submenu by using or button and press OK button.

Result: SEt flashes on the screen.

10

To exit the menu and display the Home screen, select the ESC submenu by using or button and press OK button.

Result: Home screen is displayed.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?