DOCA0160EN-00

Restoring Factory Settings

For more information, refer section Factory Settings.

Step

Action

Screen

1

Press the OK button for more than 2 s.

Result: Idn flashes on the screen.

2

Press the button two times to select SEt menu.

3

Press the OK button.

Result: Lock icon flashes and the password setting on is displayed on the screen.

4

Press the button one time to select FAC submenu.

5

Use the or button to enter the password.

6

Press the OK button.

Result: no flashes on the screen.

7

Use the or button to set the factory settings to YES.

8

Press the OK button to apply the factory settings.

Result:

  • run is displayed on the screen.

  • The factory settings of VigiPacT RHB relay are restored. After the factory settings are restored, the relay resets and the Home screen is displayed.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?