DOCA0160EN-00

Procedure

Follow the steps to perform the manual test:

  1. Press the Test button on the relay for more than 2 s.

  2. Check that the circuit breaker trips.

  3. Press the Reset button on the relay.

  4. Reset the circuit breaker.

  5. Close the circuit breaker.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?