DOCA0160EN-00

Overview

The toroids are calibrated in factory.

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION OR ARC FLASH
Turn off the main circuit breaker in the open (O) position before performing the toroid calibration.
Failure to follow these instructions will result in death or serious injury.
WARNING
HAZARD OF NON-TRIPPING
The toroid must be recalibrated:
  • following any severe electrical fault
  • periodically, once a year
Failure to follow these instructions can result in death, serious injury, or equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?