DOCA0160EN-00

Manual Test

Press and hold the Test button for more than 2 s to carry out a manual test.

The VigiPacT RHB relay:

  • simulates the detection of an alarm and activates the K1 and K2 relays. For more information, refer section Manual Test

    .
  • checks the toroid connection and settings. For more information, refer section Troubleshooting

    .

While pressing and holding the Test button, all relevant display elements are shown on the LCD display.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?