DOCA0160EN-00

Changing the Password

Step

Action

Screen

1

Press the OK button for more than 2 s.

Result: Idn flashes on the screen.

2

Press the button two times to select SEt menu.

3

Press the OK button.

Result: Lock icon flashes and the password setting on is displayed on the screen.

4

Use the and buttons to enter the password to unlock the password protection setting.

5

Press the OK button to validate the entered password.

Result: If the password is validated, the password setting on flashes on the screen.

6

Use the and buttons to set a new password.

7

Press the OK button to save the new password.

Result: Lock icon flashes and the password setting on is displayed on the screen.

8

To exit the current submenu, select the ESC submenu by using or button and press OK button.

Result: SEt flashes on the screen.

9

To exit the menu and display the Home screen, select the ESC submenu by using or button and press OK button.

Result: Home screen is displayed.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?