DOCA0160EN-00

History Memory

The history memory (HiS) menu allows you to get the value of the earth-leakage current measured for the last alarm detected and stored in the memory.

Step

Action

Screen

1

Press the OK button for more than 2 s.

Result: Idn flashes on the screen.

2

Press the button four times to select HiS menu.

3

Press the OK button.

Result: M flashes and the value of the earth-leakage current measured for the last alarm detected is displayed on the screen.

4

Press the button.

Result: When Clr flashes on the screen, the history memory can be cleared by pressing the OK button.

5

To exit the current submenu, select the ESC submenu by using or button and press OK button.

Result: HiS flashes on the screen.

6

To exit the menu and display the Home screen, select the ESC submenu by using or button and press OK button.

Result: Home screen is displayed.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?