DOCA0160EN-00

Setting ton2 Time Delay

Step

Action

Screen

1

Press the OK button for more than 2 s.

Result: Idn flashes on the screen.

2

Press the button one time to select t menu.

3

Press the OK button.

Result: ton and 2 flashes and the value of time delay ton2 is displayed on the screen.

NOTE: If the alarm threshold >I2 is set to 30 mA (protection of persons), the time delay ton2 is automatically and invariably set to 0 s.

4

Press the OK button to change the value of time delay ton2.

NOTE: If the password protection is set to on, then it is required to enter the password to change the value. Enter the password by using or button and press OK button.

5

Use the and buttons to set the appropriate value of time delay ton2.

6

Press the OK button to save the value of time delay ton2.

Result: ton and 2 flashes, and the new value of time delay ton2 is displayed on the screen.

7

To exit the current submenu, select the ESC submenu by using or button and press OK button.

Result: t flashes on the screen.

8

To exit the menu and display the Home screen, select the ESC submenu by using or button and press OK button.

Result: Home screen is displayed.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?