DOCA0160EN-00

Setting the >I1 Pre-Alarm Threshold

Step

Action

Screen

1

Press the OK button for more than 2 s.

Result: Idn flashes on the screen.

2

Press the OK button.

Result: >I2 flashes and the value of alarm threshold is displayed on the screen.

3

Press the button one time to select the pre-alarm threshold > I1 submenu.

Result: > I1 flashes and the value of pre-alarm threshold is displayed on the screen.

4

Press the OK button to change the value of pre-alarm threshold.

NOTE: If the password protection is set to on, then it is required to enter the password to change the value. Enter the password by using or button and press OK button.

5

Use the and buttons to set the appropriate value of pre-alarm threshold.

6

Press the OK button to save the value of pre-alarm threshold.

Result: >I1 flashes and the new value of pre-alarm threshold is displayed on the screen.

7

To exit the current submenu, select the ESC submenu by using or button and press OK button.

Result: Idn flashes on the screen.

8

To exit the menu and display the Home screen, select the ESC submenu by using or button and press OK button.

Result: Home screen is displayed.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?