DOCA0160EN-00

Password Management

The VigiPacT RHB relay provides password protection against unauthorised parameter changing.

The parameters are set via the menu buttons available on the VigiPacT RHB relay. When the password protection is set to on, the password is required before changing the parameter. When correct password is entered, the password is memorised until the user stays in the menu.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?