DOCA0160EN-00

Description of Screens

WARNING
HAZARD OF NON-TRIPPING
  • Protection setting adjustments must be done by qualified electrical personnel.
  • The toroid must be connected to the corresponding relay before the first use and before commissioning of the protected installation.
  • The relay must be powered prior to the protected installation.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?