Attribute Rules

DHFC employs attribute rules to perform data maintenance tasks while users are editing features. This topic describes the attribute rules, organized by dataset. Refer to Esri’s Attribute Rule Fundamentals article for more information about attribute rules.

Coax Dataset_D

There are no attribute rules applied to any features or relationships in this dataset.

Coax Dataset_A (as-built)

The polygon feature classes require the attribute rule CreateCoaxNetworkId on the NetworkId fields. DHFC requires a GUID in this field, and the attribute rule assigns one when the feature is created.

Feature Class Name

Field Name

Editing Event

Autoupdater

DoNotBuildBoundary

NetworkId

On Create

CreateCoaxNetworkId

RFNodeBoundary

NetworkId

On Create

CreateCoaxNetworkId

RFPowerSupplyBoundary

NetworkId

On Create

CreateCoaxNetworkId

Landbase Dataset

There are no attribute rules applied to any features or relationships in this dataset.

Structures Dataset

Any structure feature class (points, lines, and polygons) participating in the DHFC application requires the attribute rule CreateCoaxNetworkId on the NetworkId fields. DHFC requires a GUID in this field, and the attribute rule assigns one when the feature is created.

Feature Class Name

Field Name

Editing Event

Autoupdater

AddressPoint

NetworkId

On Create

CreateCoaxNetworkId

MduBoundary

NetworkId

On Create

CreateCoaxNetworkId

MduPathElement

NetworkId

On Create

CreateCoaxNetworkId

MduPolygonElement

NetworkId

On Create

CreateCoaxNetworkId

MduTextElement

NetworkId

On Create

CreateCoaxNetworkId

OverheadSpan

NetworkId

On Create

CreateCoaxNetworkId

RFDrop

NetworkId

On Create

CreateCoaxNetworkId

SupportStructure

NetworkId

On Create

CreateCoaxNetworkId

UndergroundJunction

NetworkId

On Create

CreateCoaxNetworkId

UndergroundSpan

NetworkId

On Create

CreateCoaxNetworkId

UndergroundStructure

NetworkId

On Create

CreateCoaxNetworkId

Refer to the Upgrade to ArcGIS Pro topic for instructions on configuring attribute rules.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?