Inline Equalizers

Inline equalizers are circuits that are situated into the front end of an amplifier or line extender to compensate for the amount of cable loss ahead of it.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?