Structures Dataset

The following tables display the required feature classes and fields that compose the Structures Dataset.

AddressPoint

<Table CoaxName="AddressPointData" EsriDesignName="AddressPoint" EsriBuiltName="AddressPoint">

This is a point feature class with the following required fields:

Field Name

Data Type

Notes

NetworkID

GUID

Unique identifier for the component or record.

ObjectID

Object ID

Esri Object Id for the feature or object.

AerialStructureId

GUID

NetworkId of the overhead structure that this component is associated with; an empty GUID means this component is not associated with any overhead structure.

CommercialMDUCount

Long Integer

The number of commercial service locations inside a Multi-Dwelling Unit (MDU)

HouseNo

String

The house number of the address point.

ResidentialMDUCount

Long Integer

The number of residential service locations inside a Multi-Dwelling Unit (MDU)

StreetName

String

The street name for the address point. This field is required for DHFC.

SymbolRotation

Double

The component’s symbol rotation.

TapId

GUID

The NetworkId of the as-built tap that feeds the address point.

TapId_D

GUID

The NetworkId of the proposed tap that feeds the address point.

UGStructureId

GUID

The NetworkId of the underground structure that this component is associated with; an empty GUID means this component is not associated with any underground structure.

MduBoundary

<Table CoaxName="MduBoundaryData" EsriDesignName="MduBoundary" EsriBuiltName="MduBoundary">

This is a polygon feature class with the following required fields:

Field Name

Data Type

Notes

NetworkID

GUID

Unique identifier for the component or record.

ObjectID

Object ID

Esri Object Id for the feature or object.

Name

String

Name of boundary

MduPathElement

<Table CoaxName="MduPathElementData" EsriDesignName="MduPathElement" EsriBuiltName="MduPathElement">

This is a line feature class with the following required fields:

Field Name

Data Type

Notes

NetworkID

GUID

Unique identifier for the component or record.

ObjectID

ObjectID

Esri Object Id for the feature or object.

MduBoundaryId

GUID

The NetworkId of the Multi-Dwelling Unit (MDU) the path element is associated with

Style

String

A .json representation of the style of the MDU element

MduPolygonElement

<Table CoaxName="MduPolygonElementData" EsriDesignName="MduPolygonElement" EsriBuiltName="MduPolygonElement">

This is a polygon feature class with the following required fields:

Field Name

Data Type

Notes

NetworkID

GUID

Unique identifier for the component or record.

ObjectID

Object ID

Esri Object Id for the feature or object.

MduBoundaryID

GUID

The NetworkId of the Multi-Dwelling Unit (MDU) the polygon element is associated with

Style

String

A .json representation of the style of the MDU element

MduTextElement

<Table CoaxName="MduTextElementData" EsriDesignName="MduTextElement" EsriBuiltName="MduTextElement">

This is a point feature class with the following required fields:

Field Name

Data Type

Notes

NetworkID

GUID

Unique identifier for the component or record.

ObjectID

Object ID

Esri Object Id for the feature or object.

MduBoundaryId

GUID

The NetworkId of the Multi-Dwelling Unit (MDU) the text element is associated with

Style

String

A .json representation of the style of the MDU element

Text

String

The text to be displayed

OverheadSpan

<Table CoaxName="OverheadSpanData" EsriDesignName="OverheadSpan" EsriBuiltName="OverheadSpan">

This is a line feature class with the following required fields:

Field Name

Data Type

Notes

NetworkID

GUID

Unique identifier for the component or record.

ObjectID

Object ID

Esri Object Id for the feature or object.

IsInMDU

Short Integer

Boolean (typically Yes/No) indicating whether or not the component is found within an Multi-Dwelling Unit (MDU).

Length

Double

The length of the span; this value is automatically provided by DHFC based on the strand length, but it can be overridden by the user

RFDrop

<Table CoaxName="RFDropData" EsriDesignName="RFDrop" EsriBuiltName="RFDrop">

This is a line feature class with the following required fields:

Field Name

Data Type

Notes

NetworkID

GUID

Unique identifier for the component or record.

ObjectID

Object ID

Esri Object Id for the feature or object.

Workflow_Status

String

WorkflowState enumeration: AsBuilt and Proposed; for more information, refer to the topic Enumerated Data Types.

SupportStructure

<Table CoaxName="SupportStructureData" EsriDesignName="SupportStructure" EsriBuiltName="SupportStructure">

This is a point feature class with the following required fields:

Field Name

Data Type

Notes

NetworkID

GUID

Unique identifier for the component or record.

ObjectID

Object ID

Esri Object Id for the feature or object.

CommercialCount

Integer

The number of commercial service locations associated with the structure

IsInMDU

Short Integer

Boolean (typically Yes/No) indicating whether or not the component is found within an Multi-Dwelling Unit (MDU).

PoleType

Short Integer

The application requires the following four values: CableOnly, PowerAndPhone, MidSpan, and Demarcation. Beyond that, other values may be added to the coded value domain and mapped to the GIS domain. See the topic Schema.xml Configuration File for more information.

ResidentialCount

Long Integer

The number of residential service locations associated with the structure

RiserDistance

Double

The height of a riser, if one is present

SymbolRotation

Double

The component’s symbol rotation.

UndergroundJunction

 <Table CoaxName="RFUndergroundJunctionData" EsriDesignName="RFUndergroundJunction" EsriBuiltName="RFUndergroundJunction">

This is a point feature class with the following required fields:

Field Name

Data Type

Notes

NetworkID

GUID

Unique identifier for the component or record.

ObjectID

Object ID

Esri Object Id for the feature or object.

IsInMDU

Short Integer

Boolean (typically Yes/No) indicating whether or not the component is found within an Multi-Dwelling Unit (MDU).

SymbolRotation

Double

The component’s symbol rotation.

Type

Short Integer

UndergroundJunctionType enumeration: SharpTurn, BoreHole; for more information, see the topic Enumerated Data Types

UndergroundSpan

<Table CoaxName="UndergroundSpanData" EsriDesignName="UndergroundSpan" EsriBuiltName="UndergroundSpan">

This is a line feature class with the following required fields:

Field Name

Data Type

Notes

NetworkID

GUID

Unique identifier for the component or record.

ObjectID

Object ID

Esri Object Id for the feature or object.

IsInMDU

Short Integer

Boolean (typically Yes/No) indicating whether or not the component is found within an Multi-Dwelling Unit (MDU).

Length

Double

The length of the underground span

UndergroundStructure

<Table CoaxName="UndergroundStructureData" EsriDesignName="UndergroundStructure" EsriBuiltName="UndergroundStructure">

This is a point feature class with the following required fields:

Field Name

Data Type

Notes

NetworkID

GUID

Unique identifier for the component or record.

ObjectID

Object ID

Esri Object Id for the feature or object.

CommercialCount

Short Integer

The number of commercial service locations associated with the structure

IsInMDU

Short Integer

Boolean (typically Yes/No) indicating whether or not the component is found within an Multi-Dwelling Unit (MDU).

ResidentialCount

Long Integer

The number of residential service locations associated with the structure

StructureType

String

The type of underground structure the component represents; DHFC handles the types Demarcation and AptBox with specific functionality, and all other structure types are treated as the same generic structure; all structure type values should correspond to a defined Underground Structure Type from a DHFC catalog spec

SymbolRotation

Double

The component’s symbol rotation.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?