Taps

Taps are installed in the distribution cable to divert a portion of the downstream distribution signal and split it to feed typically two to eight individual subscribers. In the reverse direction, it combines the signal from subscribers and inserts it into the upstream direction of the distribution cable.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?