RFCable_OverheadSpan
There are two versions of this attributed relationship:
-
RFCable_OverheadSpan for the as-built representation.
-
RFCable_OverheadSpan_D for the design representation.
RFCable_OverheadSpan, the As-Built Relationship
|
Relationship Class Property |
Value or Choice |
|---|---|
|
Name |
RFCable_OverheadSpan |
|
Origin Table or Feature Class |
RFCable |
|
Destination Table or Feature Class |
OverheadSpan |
|
Relationship Type |
Simple |
|
Forward Label |
OverheadSpan |
|
Backward Label |
RFCable |
|
Message Direction |
None (no messages propagated) |
|
Cardinality |
M-N (many to many) |
|
Attributed |
Check the box for “Relationship class is attributed.” After the relationship is created, you then add attribute fields to the table. Refer to the Add Attribute Fields to Relationship Tables for more information. |
|
Origin Primary Key |
NetworkId |
|
Origin Foreign Key |
RFCableNetworkId |
|
Destination Primary Key |
NetworkId |
|
Destination Foreign Key |
OverheadSpanNetworkId |
RFCable_OverheadSpan_D, the Design Relationship
|
Relationship Class Property |
Value or Choice |
|---|---|
|
Name |
RFCable_OverheadSpan_D |
|
Origin Table or Feature Class |
RFCable_D |
|
Destination Table or Feature Class |
OverheadSpan |
|
Relationship Type |
Simple |
|
Forward Label |
OverheadSpan |
|
Backward Label |
RFCable_D |
|
Message Direction |
None (no messages propagated) |
|
Cardinality |
M-N (many to many) |
|
Attributed |
Check the box for “Relationship class is attributed.” After the relationship is created, you then add attribute fields to the table. Refer to the Add Attribute Fields to Relationship Tables for more information. |
|
Origin Primary Key |
NetworkId |
|
Origin Foreign Key |
RFCableNetworkId |
|
Destination Primary Key |
NetworkId |
|
Destination Foreign Key |
OverheadSpanNetworkId |