Configure the Geodatabase

As stated in the Perform Solution Center Configurations topic, an early procedure in the process is to ensure your geodatabase is ready to support DHFC. The majority of configuration work happens in parallel with finishing your equipment catalogue in Solution Center.

The underlying geodatabase must contain certain feature classes, tables, and relationships, along with sets of required fields and properties. The topics in this section detail these requirements, beginning with feature classes, then tables, and finally relationships.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?