Amplifier Internal Equalizers

Amplifier internal equalizers reverse the non-linear attenuation of frequencies that the coaxial path causes, attenuating only the low-band to restore a degree of linearity or positive slope between hyper and low band frequencies.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?