Attenuator Plugin

Attenuator plugins are used to reduce the electrical signal strength. They are only used by an In Line Equalizer Reverse Conditioner (LEQ/RC). Further, this attenuator only applies to the return path, so it does not affect downstream components.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?