Segmentable Nodes

Much like a standard node, segmentable nodes receive the linearly modulated frequency division multiplexing (FDM) spectrum, converting the signal back to RF form before transmitting it into one or more coaxial distribution legs. However, in a segmentable node, the forward path is able to be segmented via independent optical receivers that supply dedicated ports.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?