RFNodeCoaxPort / RFNodeCoaxPort_D (RFNodeCoaxPortData)
DHFC object name: RFNodeCoaxPortData
GIS design table name: RFNodeCoaxPort_D
GIS built table name: RFNodeCoaxPort
GIS table type: ObjectClass
Geometry type: Any
Fields
|
Name |
Alias |
Type |
Domain |
Length |
Precision |
Nullable |
Field Role |
Data Transfer |
|---|---|---|---|---|---|---|---|---|
|
ConnectedItemId |
ConnectedItemId |
Guid |
FALSE |
Required |
BiDirectional |
|||
|
EsriId |
OBJECTID |
ObjectId |
FALSE |
Required |
BiDirectional |
|||
|
IsPowerOnly |
Is Power Only |
SmallInteger |
EsriYesNoEnum |
FALSE |
Required |
BiDirectional |
||
|
NetworkId |
NetworkId |
String |
200 |
FALSE |
Required |
BiDirectional |
||
|
NodeId |
NodeId |
Guid |
FALSE |
Required |
BiDirectional |
|||
|
PortNumber |
Port Number |
SmallInteger |
FALSE |
Required |
BiDirectional |
|||
|
Workflow_Status |
Workflow Status |
String |
WorkflowState |
FALSE |
Required |
BiDirectional |
||
|
CreationUser |
Creation User |
String |
50 |
TRUE |
Optional |
BiDirectional |
||
|
DateCreated |
Date Created |
Date |
TRUE |
Optional |
BiDirectional |
|||
|
DateModified |
Date Modified |
Date |
TRUE |
Optional |
BiDirectional |
|||
|
HomesPassed |
Homes Passed |
Integer |
TRUE |
Optional |
ToGisOnly |
|||
|
LastUser |
Last User |
String |
50 |
TRUE |
Optional |
BiDirectional |
||
|
PortName |
Port Name |
String |
5 |
TRUE |
Optional |
ToGisOnly |
Required Fields
|
Field Name |
Notes |
|---|---|
|
NetworkID |
Unique identifier for the component or record. |
|
ObjectID |
Esri Object Id for the feature or object. |
|
GlobalID |
Esri Global ID for the feature or object. |
|
ConnectItemId |
The NetworkId of the component that is connected downstream to the amplifier on the specified port. |
|
NodeId |
The NetworkId of the node to which this port data corresponds. |
|
PortNumber |
The port number on the component to which t the connection data applies. |
|
Workflow_Status |
WorkflowState enumeration: AsBuilt and Proposed; for more information, refer to the topic Enumerated Data Types. |
Relationships
None.