RFPowerInserterPort / RFPowerInserterPort_D (RFPowerInserterPortData)
DHFC object name: RFPowerInserterPortData
GIS design table name: RFPowerInserterPort_D
GIS built table name: RFPowerInserterPort
GIS table type: ObjectClass
Geometry type: Any
Fields
|
Name |
Alias |
Type |
Domain |
Length |
Precision |
Nullable |
Field Role |
Data Transfer |
|---|---|---|---|---|---|---|---|---|
|
ConnectedItemId |
ConnectedItemId |
Guid |
FALSE |
Required |
BiDirectional |
|||
|
EsriId |
OBJECTID |
ObjectId |
FALSE |
Required |
BiDirectional |
|||
|
NetworkId |
NetworkId |
String |
200 |
FALSE |
Required |
BiDirectional |
||
|
PortNumber |
Port Number |
SmallInteger |
FALSE |
Required |
BiDirectional |
|||
|
PowerInserterId |
PowerInserterId |
Guid |
FALSE |
Required |
BiDirectional |
|||
|
Workflow_Status |
Workflow Status |
String |
WorkflowState |
FALSE |
Required |
BiDirectional |
||
|
CreationUser |
Creation User |
String |
50 |
TRUE |
Optional |
BiDirectional |
||
|
DateCreated |
Date Created |
Date |
TRUE |
Optional |
BiDirectional |
|||
|
DateModified |
Date Modified |
Date |
TRUE |
Optional |
BiDirectional |
|||
|
LastUser |
Last User |
String |
50 |
TRUE |
Optional |
BiDirectional |
Required Fields
|
Field Name |
Notes |
|---|---|
|
NetworkID |
Unique identifier for the component or record. |
|
ObjectID |
Esri Object Id for the feature or object. |
|
GlobalID |
Esri Global ID for the feature or object. |
|
ConnectedItemId |
The NetworkId of the component the power inserter is connected to on the given port. |
|
PortNumber |
The port number on the component to which t the connection data applies. |
|
PowerInserterId |
The ID of the power inserter component. |
|
Workflow_Status |
WorkflowState enumeration: AsBuilt and Proposed; for more information, refer to the topic Enumerated Data Types. |
Relationships
None.