Perform Solution Center Configuration

Configuring your equipment catalogue early in the process is essential for a successful implementation. Some of the configuration is completed in DHFC and the rest in Solution Center. To properly configure DHFC, you work with Solution Center in tandem with configuring the geodatabase (using the Configure the Geodatabase help topics).

Several elements of configuration performed in Solution Center include:

  • Managing the equipment catalog.

  • Connecting the DHFC application to the published map service.

  • Building reference maps for end users.

  • Controlling tombstone printing.

  • Choosing units of measure.

  • Uploading the schema.xml.

  • Exporting the equipment catalogue to Excel.

  • Importing the equipment catalogue from Excel.

In Solution Center, select the DHFC plugin to get started.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?