RFPowerInserter_RFPowerInserterPort
There are two versions of this relationship:
-
RFPowerInserter_RFPowerInserterPort for the as-built representation.
-
RFPowerInserter_RFPowerInserterPort_D for the design representation.
RFPowerInserter_RFPowerInserterPort, the As-Built Relationship
|
Relationship Class Property |
Value or Choice |
|---|---|
|
Name |
RFPowerInserter_RFPowerInserterPort |
|
Origin Table or Feature Class |
RFPowerInserter |
|
Destination Table or Feature Class |
RFPowerInserterPort |
|
Relationship Type |
Simple |
|
Forward Label |
RFPowerInserterPort
IMPORTANT: The Forward Label
you type while creating the relationship must match the EsriBuiltName
entry in the schema.xml file for this component.
|
|
Backward Label |
RFPowerInserter |
|
Message Direction |
None (no messages propagated) |
|
Cardinality |
1–M (one to many) |
|
Relationship Attributes |
No, I do not want to add attributes to this relationship class. |
|
Primary Key |
NetworkId |
|
Foreign Key |
PowerInserterId |
RFPowerInserter_RFPowerInserterPort _D, the Design Relationship
|
Relationship Class Property |
Value or Choice |
|---|---|
|
Name |
RFPowerInserter_RFPowerInserterPort_D |
|
Origin Table or Feature Class |
RFPowerInserter_D |
|
Destination Table or Feature Class |
RFPowerInserterPort_D |
|
Relationship Type |
Simple |
|
Forward Label |
SECom.ARCFM.RFPowerInserterPort
IMPORTANT: The
Forward Label you type while creating the relationship must match
the EsriDesignName entry in the schema.xml file for this component.
|
|
Backward Label |
SECom.ARCFM.RFPowerInserter |
|
Message Direction |
None (no messages propagated) |
|
Cardinality |
1–M (one to many) |
|
Relationship Attributes |
No, I do not want to add attributes to this relationship class. |
|
Primary Key |
NetworkId |
|
Foreign Key |
PowerInserterId |