RFPad / RFPad_D (RFPadData)
DHFC object name: RFPadData
GIS design table name: RFPad_D
GIS built table name: RFPad
GIS table type: ObjectClass
Geometry type: Any
Fields
|
Name |
Alias |
Type |
Domain |
Length |
Precision |
Nullable |
Field Role |
Data Transfer |
|---|---|---|---|---|---|---|---|---|
|
CatalogId |
CatalogId |
Guid |
FALSE |
Required |
BiDirectional |
|||
|
EsriId |
OBJECTID |
ObjectId |
FALSE |
Required |
BiDirectional |
|||
|
ModelNumber |
Model Number |
String |
50 |
TRUE |
Required |
BiDirectional |
||
|
NetworkId |
NetworkId |
String |
200 |
FALSE |
Required |
BiDirectional |
||
|
Workflow_Status |
Workflow Status |
String |
WorkflowState |
FALSE |
Required |
BiDirectional |
||
|
CreationUser |
Creation User |
String |
50 |
TRUE |
Optional |
BiDirectional |
||
|
DateCreated |
Date Created |
Date |
TRUE |
Optional |
BiDirectional |
|||
|
DateModified |
Date Modified |
Date |
TRUE |
Optional |
BiDirectional |
|||
|
Direction |
Direction |
SmallInteger |
ForwardReturnDomain |
TRUE |
Optional |
ToGisOnly |
||
|
InventoryNum |
Inventory Number |
String |
50 |
TRUE |
Optional |
ToGisOnly |
||
|
LastUser |
Last User |
String |
50 |
TRUE |
Optional |
BiDirectional |
||
|
Manufacturer |
Manufacturer |
String |
50 |
TRUE |
Optional |
ToGisOnly |
||
|
Value |
Pad Value |
String |
50 |
TRUE |
Optional |
ToGisOnly |
Required Fields
|
Field Name |
Notes |
|---|---|
|
NetworkID |
Unique identifier for the component or record. |
|
ObjectID |
Esri Object Id for the feature or object. |
|
GlobalID |
Esri Global ID for the feature or object. |
|
CatalogId |
The Id of the DHFC catalog spec associated with the component; should be a string representation of a valid GUID in the following format, 6A1F97AD-C665-4521-B954-29A4429FC128. |
|
ModelNumber |
The component model number. |
|
Workflow_Status |
WorkflowState enumeration: AsBuilt and Proposed; for more information, refer to the topic Enumerated Data Types. |
Relationships