RFCoupler_RFCouplerPort
There are two versions of this relationship:
-
RFCoupler_RFCouplerPort for the as-built representation.
-
RFCoupler_RFCouplerPort_D for the design representation.
RFCoupler_RFCouplerPort, the As-Built Relationship
|
Relationship Class Property |
Value or Choice |
|---|---|
|
Name |
RFCoupler_RFCouplerPort |
|
Origin Table or Feature Class |
RFCoupler |
|
Destination Table or Feature Class |
RFCouplerPort |
|
Relationship Type |
Simple |
|
Forward Label |
RFCouplerPort |
|
Backward Label |
RFCoupler |
|
Message Direction |
None (no messages propagated) |
|
Cardinality |
1–M (one to many) |
|
Relationship Attributes |
No, I do not want to add attributes to this relationship class. |
|
Primary Key |
NetworkId |
|
Foreign Key |
CouplerId |
RFCoupler_RFCouplerPort_D, the Design Relationship
|
Relationship Class Property |
Value or Choice |
|---|---|
|
Name |
RFCoupler_RFCouplerPort_D |
|
Origin Table or Feature Class |
RFCoupler_D |
|
Destination Table or Feature Class |
RFCouplerPort_D |
|
Relationship Type |
Simple |
|
Forward Label |
SECom.ARCFM.RFCouplerPort |
|
Backward Label |
SECom.ARCFM.RFCoupler |
|
Message Direction |
None (no messages propagated) |
|
Cardinality |
1–M (one to many) |
|
Relationship Attributes |
No, I do not want to add attributes to this relationship class. |
|
Primary Key |
NetworkId |
|
Foreign Key |
CouplerId |